大家好,如何控制LMH6525快速控制Laser Diode(650nm 5mw)亮灭亮灭,需要把晶振开起来吗,求指导,
liuyunbing@ravalley.com.cn
,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
大家好,如何控制LMH6525快速控制Laser Diode(650nm 5mw)亮灭亮灭,需要把晶振开起来吗,求指导,
liuyunbing@ravalley.com.cn
,谢谢
1、第一种情况是 ENABLE 和 ENR 都一直是高电平是吗?
2、交换ENR和ENABLE方式,是指ENABLE 输入高电平;ENR输入PWM 是吗?您这里输入的PWM 频率是多少?
1、第一种情况是 ENABLE是1KHZ PWM;ENR一直是高电平
2、第二种情况是 ENABLE是高电平(现接3.3V) ;ENR一直是PWM,频率是200KHZ,今天把晶振功能开启了,有电流输出(约22ma)。
3、有个新的问题请教,ENR接的3.3V电平,ENABLE我现在接的2.5V电平,ENABLE最大能接多少电平。 我现在IR那组电流,我I2,I3,I4的电流还没有叠加使用,如果只使用IR这组电流,调节IR的输入电阻(图中的R1),最大能够输出多大电流。
谢谢

1、根据下面真值表,Iout输出和Oscillator输出是2种控制方式,我看datasheet ENABLE是高电平,ENR是PWM,应该也可以输出的,您可以测量下输入的控制信号吗?看看是否存在异常?

3、ENR和ENABLE的控制电平,如下datasheet,这里的max与min 应该反了,这样ENABLE最大电压是2.8V,ENR最大电平是2V,因此,您还不可以ENR接3.3V电平

IR这一通道最大输出电流150mA,注意通道增益是150,因此最大输入电流是1mA