This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83867IS: SGMII接口通讯

Part Number: DP83867IS

大家好,我现在使用DP83867和sgmii,电脑和FPGA开发板用网线直连,一上电我把DP83867SGMII_en拉高,并且配置成六线sgmii模式,但是SGMII_SOP和SGMII_SON时钟无法提供时钟,这是怎么回事?

  • 您好,SGMII_COP和SGMII_CON 是SGMII clock输出,SGMII_SOP 和SGMII_SON是SGMII data output。

    这四个引脚都有输出吗?

    建议附上电路图看下。

  • 您好,我现在无法SGMII_SOP 和SGMII_SON是SGMII data output两对差分线是否有输出,因为不能在线debug,能确定的是vivadoIP核1G/2.5G PCS/PMA or SGMII的状态会由16‘h0800变成16’h0810,不明原因又会变成16‘h0800。像是DP83867这个芯片在经过我的配置后,又被复位了,我对他的配置被清空,但是我代码并没有把它复位,很疑惑

  • 您好,不能判断引脚是否有输出,不能debug,能读取它的寄存器吗?

    DP83867 经过配置,然后被复位,所有寄存器都恢复到默认值?也就是说无法对DP83867的寄存器进行配置是吧?