This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1044V-Q1: 这颗和TCAN1044-Q1有什么区别呢

Part Number: TCAN1044V-Q1
Other Parts Discussed in Thread: TCAN1044-Q1

TCAN1044V-Q1和TCAN1044-Q1区别是什么呢

  • 您好,后缀V版本和不带V的区别在于pin5, 带V的pin 5是Vio:Supply voltage for I/O level shifter。 可以看到它的电压范围为1.7V到5.5V,也就是说逻辑控制引脚STB,RXD, TXD这几个引脚可以使用不同的逻辑电平和MCU接,比如1.8V VIO会使得控制引脚STB,RXD和TXD的电平也为1.8V,免去使用电平转换器件。