This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI:
输入为2*4lane DSI,输出FPD LINK信号,外设解串以后支持4K分辨率的显示器。请问是用两颗输入为4lane的的芯片吗?请推荐一下实现方案。谢谢~~
您好,您可以直接考虑双路DSI input的DS90UB941AS,每路都能支持到4lane DSI 输入,您看下它的数据手册:
您好不能达到4k 60fps分辨率,941AS的像素时钟最大210MHz为3K 30fps分辨率。
并且我看了下目前输入兼容DSI输入的,最大像素时钟和941AS一样为210MHz。