This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TUSB320: TUSB320技术问题

Part Number: TUSB320


我们想实现:带IIC/带OTG输出的充电管理+DRP这个功能,我们TYPE C只支持USB2.0,不支持3.0

1.TUSB320的TYPEC口能实现5V/3A充电吗,如果更高的电压能支持实现OTG U盘的识别吗?

2.INT_N在哪种状态下为L?识别到哪种设备?

3. 正常冲i但插入适配器不管多少V,都只能识别5V, 请问使用TUSB320通过软件能实现吗?如何实现?

  • 您好,

    1)对于 Type-C 、 DFP 端口只能提供功率水平并高达该电流(only advised)。 UFP 端口负责消耗功能所需的电流。 TUSB320 应仅通过 ID 引脚 / 功能控制 Vbus 电源开关使能引脚、而不影响提供的负载电流。 请参考下下 Type-C 规范 (2.3.4 USB Type-C VBUS 电流检测和使用):

    USB Type-C Current at either 1.5 A or 3.0 A is primarily intended for charging applications. The Sink can vary its current draw up to the advertised limit. Offering USB Type-C Current at either 1.5 A or 3.0 A is allowed for a host providing bus power to a device. The host needs to assume that the device will continuous ly draw up to
    the offered limit.

    简而言之,并非所有 Type-C 负载都将消耗 ~3A。 为了确保 TUSB320 实现3A功能,您应该测量三个方面:

    1)VDD 大于 3.5V

    2)当存在 Rd 时、 CC 电压在 ~1.31V - 2.04V (VRD-3.0) 之间 Table 4-36 Voltage on Sink CC pins (Multiple Source Current Advertisements))

    3)当向 CC 检测到 Rd 时、 ID 为低电平 (建立有效连接)。

    2. INT_N当作为中断引脚功能时,如果寄存器的信息更新,产生中断,此引脚会被拉低。

    3. VDD最大电压是5V. 您的意思是USB Vbus电压范围会达到5.25V,但是VDD最大只能5V是吗? 这个是没办法的。