Part Number: DS90UB925QSEVB
Other Parts Discussed in Thread: DS90UB925Q-Q1
925/948工作在repeater模式下,主机端已经可以获取到触摸屏数据,但是触摸屏的中断信号传递,925的INTB引脚到主机量不到信号变化。
请问如果要透传中断信号,925和948需要怎么配置呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB925QSEVB
Other Parts Discussed in Thread: DS90UB925Q-Q1
925/948工作在repeater模式下,主机端已经可以获取到触摸屏数据,但是触摸屏的中断信号传递,925的INTB引脚到主机量不到信号变化。
请问如果要透传中断信号,925和948需要怎么配置呢?

您好,INTB应该不可以透传。
我想您可以 通过GPIO透传。将触摸屏的INT信号接948的GPIO信号,948的GPIO配置为input,925的GPIO配置为output。
但是需要注意,和925搭配时候, 948必须配置围为18 bit mode, 才允许GPIO透传到925端。
Note: if paired with a DS90UB925Q-Q1 serializer, the devices must be configured into 18-bit mode to allow usage of GPIO pins on the serializer。