Other Parts Discussed in Thread: DS90UB927Q-Q1,


1)0X65寄存器配置为0X03,
2)0X39 配置为0X02,
3)0X64 配置为0X11.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.



您好,建议按照datasheet先做个BIST自检测试,看下Pass和lock引脚是否都正常。
如果BIST测试通过,说明927和928之间的link是没问题的。
框架还漏了CPU+927+928+ML86177(罗姆芯片)+ TFT显示屏 现在测试结果是lock信号一直是高电平 ;目前在做BIST检测时,因为芯片上BISTC悬空状态,BISTEN被拉低了。不太好设置,故设置BIST寄存器来检测 现在设置的是将0x24 设置成0x01:BIST Pin Configuration Config 0: BIST enabled from register ;BIST Control 1: Enabled,但是实际结果为Pass一直检测到低电平,而且配置之后IIC通讯异常,想请问下是否是寄存器配置的还有问题,或者还要配置其他寄存器 下图为928芯片配置图
抱歉回复晚了。
0x02配置成0x90,即bit4=1. bit4的含义是输出sleep状态的选择控制。 当为0的时候,disable output sleep,当配置为1的时候,output sleep enable。
所以这位应该配置为0,也即默认配置,三态输出,如果配置为1,说明enable sleep。 因此没有输出,并且OSS_SEL引脚也不会拉高。