This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA9543A: TCA9543A Issue discussion

Part Number: TCA9543A



Dear TEAM,

1.芯片是否為通過寄存器控制Channel 0,Channel 1 開關。(See attached file: TCA9543A datasheet.pdf)

2.芯片SDX,SCX輸出是否需要串聯電阻以減少干擾。


3.Pin INT1,INT2 NC 是否會影響Channel 0 Channel1輸出。
 
Regards,

bard 

  • 您好,

    1、是的,通过Control 寄存器确定要选择的通道;然后就可以与选择的通道进行I2C通信了。

    2、可以预留电阻位置,待调试时选择合适的电阻值;

    3、Pin INT1,INT2如果不用,需要通过上拉电阻连接到VCC。