Part Number: DS90UB953-Q1
目前使用DS90UB953+DS90UB960搭配,想要在DS90UB953这边配置Pateern输出,按照953的spec中的code example对953进行如下配置:

预期应该显示出2560*720@30fps的pattern,但目前直接取960的输出进行显示是黑屏,请问可能是什么原因呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB953-Q1
目前使用DS90UB953+DS90UB960搭配,想要在DS90UB953这边配置Pateern输出,按照953的spec中的code example对953进行如下配置:

预期应该显示出2560*720@30fps的pattern,但目前直接取960的输出进行显示是黑屏,请问可能是什么原因呢?
您好,
关于您的这个问题,我已将它发布在E2E英文论坛,如下链接,请等待E2E论坛工程师的回复:
E2E工程师已给予回复:
Have you tried using the patgen on the 960 side? It would be good to know what side of the link the problem is on. If you are able to pull all the registers from the 960 as well I would like to verify the CSI forwarding is configured correctly.
In the meantime what you could also check is that the 960 is receiving data by reading registers 0x73 - 0x76 for the port that 953 is connected to. Also verify you are forwarding that data from the RX port to the correct CSI port by looking at registers 0x20 and 0x33.
对应的中文是:
你试过在960侧使用 Pattern 吗?最好知道问题在哪一方。您是否可以从960中提取所有寄存器,我想验证CSI forwarding 配置是否正确。
同时,您还可以通过读取寄存器0x73-0x76检查960是否在接收953所连接端口的数据。另外,通过查看寄存器0x20和0x33,验证您正在将该数据从RX端口转发到正确的CSI端口。
如果您的问题还未解决,请跟进E2E工程师的回复。
您好,非常感谢您的帮助。我的问题已得到解决,原因如下:
953 spec中只提到了RGB888的配置,而960是客户端进行调试,没有确认清楚色彩格式,实际上需要配置的是YUV422的pattern
后来在https://e2e.ti.com/support/interface-group/interface/f/interface-forum/790989/ds90ub953-q1-pattern-generation-for-yuv422?tisearch=e2e-sitesearch&keymatch=ds90ub953%25252525252525252520pattern#这篇回答下确认了YUV422 pattern配置的方法,已经成功输出color bar