hi;
你好,我现在想提高输出电流,我想用多个通道叠加起来,我改变IR输入电阻,电流输出大小可以改变,如果IR通道电阻固定后,通过FPGA的IO口输出差分信号(3.3V高电平,低电平0v)控制EN2+,EN2B-时候,这个时候电流没有叠加上来,把EN2+,EN2B-两个引脚断开,电流输出端190mA电流,没有办法断开电流(意思是高速开关开关),请教如何操作,能使电流达到200mA以上而且可以快速关闭,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi;
你好,我现在想提高输出电流,我想用多个通道叠加起来,我改变IR输入电阻,电流输出大小可以改变,如果IR通道电阻固定后,通过FPGA的IO口输出差分信号(3.3V高电平,低电平0v)控制EN2+,EN2B-时候,这个时候电流没有叠加上来,把EN2+,EN2B-两个引脚断开,电流输出端190mA电流,没有办法断开电流(意思是高速开关开关),请教如何操作,能使电流达到200mA以上而且可以快速关闭,谢谢
您好,
关于这个问题,我看到在E2E英文论坛有类似的帖子,请您等待E2E英文论坛工程师的回复: