This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCAN1042-Q1: TCAN1042 AND TCAN1044 POWER ON QUESTION

Part Number: TCAN1042-Q1


TCAN1042 AND TCAN1044 POWER ON QUESTION

还是关于1042或1044的问题,我想问问,此芯片有VIO和VCC模式,我MCU控制是3.3V的。如果我系统上电,有没有时序要求,我的意思是,如果我先VCC上电了,但是我VIO等了很久才上电,此时系统有没影响呢,比如像STB这个信号,受我MCU控制,会不会造成误触发CAN输出。还是说芯片对VIO和VCC上电时间有要求,因为我在数据手册没看到相关介绍,谢谢。我同时在对比NXP的TJA1042,它是没有这个VIO悬空的模式的。

  • 您好,

    带V后缀的产品才有VIO管脚,看下面关于VCC和VIO欠压的保护表格,如果VCC先上电了,VIO等了很久才上电,那么这段时间是表格中的第3种情况,设备进入保护状态。

    其他的上电顺序也可以从表格中找出相应的设备状态。具体说明在数据手册 9.3.3 Undervoltage Lockout部分。

  • 是的,不好意思哈,我手册没看清楚,你们的NC和VIO是2个不同版本的东西,我以为是自动检测VIO和NC。谢谢。