你好,我们使用ds90ub960 -> 953 -> imx390的mipi csi链路,现在进行了配置,可以访问到953的i2c设备,写390也是正常的,但是读390一直出差,390要进行怎么样的配置,或者960和953要进行怎么样的配置?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我们使用ds90ub960 -> 953 -> imx390的mipi csi链路,现在进行了配置,可以访问到953的i2c设备,写390也是正常的,但是读390一直出差,390要进行怎么样的配置,或者960和953要进行怎么样的配置?
您好,390的地址是多少,和390通信,只需要配置960的slave ID和slave Alias ID就好。 Slave ID和Slave Alias ID 地址可以配置为相同的。
你好,安装SDK中的说明,390的地址是
#if (CAM_MODULE_VER == 0)
#define IMX390_I2C_ADDR 0x42
#elif (CAM_MODULE_VER == 1)
#define IMX390_I2C_ADDR 0x34
#else
slave ID和Alias ID也都配置了
slave ID和Alias ID也都配置了
配置的0x5d和0x65吗?分别配置的多少。
0x5c 0x30 //串行器的ID
0x5d 0x34 //sensor的ID
0x65 0x34 //sensor的别名
390的7bit从机地址是不是0011010? 如果写地址是0x34,那么读取的时候第8bit应该是1,即地址为0x35。