This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI专家您好:
测试发现这个情况,如果这个TVS管损坏,对地阻抗100欧姆左右,无法通信。
原理图中R78没有焊接。
问一下485AB口内部的驱动方式是怎样设计的;如果是强驱动,AB口对地有一百欧姆左右的对地阻抗是不影响通讯的,但实测对地有一百欧姆阻抗后,电平无法上拉。
您好,
AB口内部的驱动电路如下截图红色框内所示:
B线对地阻抗100欧姆左右时,从下图可以看出,A和B的差分电压VD是会受到这个对地100Ω影响的,特别是在后一种情况,A和B的差分电压为-VD时:
您好,我这还想请教下::
1、VF和VR-on的幅值大概多大?晶体管导通阻抗有多大?
即使B口对地100欧姆,除非晶体管内阻很大,否则BA直接差分电压能满足大于200mV