各位好,
现SOC只支持输出RGB565,能否通过DS90UB925转成LVDS输出
DS90UB925的数据使能脚(DE)要怎么接?
或者TI有没有别的串行器能实现RGB565转LVDS,大家有没有推荐?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好,
现SOC只支持输出RGB565,能否通过DS90UB925转成LVDS输出
DS90UB925的数据使能脚(DE)要怎么接?
或者TI有没有别的串行器能实现RGB565转LVDS,大家有没有推荐?
您好, 925 可以支持RGB565 输入格式,您可以只是用高几位,其余不用的bit可直接悬空即可。
另外,DE的话,可直接下拉接GND。
好的,谢谢。
另外想请教一下,如果DE不使用的话,需要对925的寄存器进行配置吗?
您好,根据DE信号的定义:Video control signal pulse width must be 3 PCLKs or longer to be transmitted when the Control Signal Filter is enabled. There is no restriction on the minimum transition pulse when the Control Signal Filter is disabled. The signal is limited to 2 transitions per 130 PCLKs.
所以当信号滤波器enable时,视频控制信号脉冲有要求,所以如果DE不使用的话,可以将control signal filter disable。即寄存器0x03 bit4=0, 即filter disable。