你好,我想了解下TCAN1046是怎么支持IO为1.8V电压的呢。。你们手册定义下没有VIO,2个通道都是一个独立电源,而应用第一页写了支持1.8V.。。。。。。。我的理解是不是VCC可以给1.8V?但是你们定义VCC为4.5V到5.5V
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我想了解下TCAN1046是怎么支持IO为1.8V电压的呢。。你们手册定义下没有VIO,2个通道都是一个独立电源,而应用第一页写了支持1.8V.。。。。。。。我的理解是不是VCC可以给1.8V?但是你们定义VCC为4.5V到5.5V
您好,感谢您的反馈,是的,TCAN1046没有VIO这个引脚,这句介绍应该是没有的,并且VCC只能支持4.5V~5.5V电压,所以TX和RX的电压是参考VCC的。
其他器件i比如TCAN1043是有VIO这个引脚的,也就是指的VIO pin的电压范围。给您造成误解非常抱歉。