This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB947-Q1: 与串行器连接输出通道问题

Part Number: DS90UB947-Q1

hello expert:

目前我们在使用947输出DOUT1与948RIN0连接,无法显示图像。

947使用单通道与948连接,串行器947输出DOUT0 是否一定要与解串器948RIN0通道相连才能正常工作?

  • 您好,947 使用single link是吗?那么建议配置auto detection operation。 寄存器DUAL_CTL1 bit2=0.

    如果是dual link 操作的话,并且不使用auto detection,那么寄存器DUAL_CTL1 bit6应该是针对DOUT1和RIN0,或者DOUT0 和RIN1交换连接的配置。

    您这边试试,看是否能解决您的问题,如果不能,再联系。