This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以将这句话拆开几层意思来理解:
首先ISO1176这是一款隔离器。
第二,带隔离功能的差分Data-line的收发器。
第三,这款隔离的收发器内部集成了晶振。可以参考datasheet Page1的内部架构,D1和D2连接一个OSC。
第四,D1和D2可以作为输入端,经过隔离变压器之后作为信号的输入端,结合datasheet 中的Figure1的应用框图你就可以理解这两个引脚的作用了。
D1和D2是输入吗?我怎么感觉是输出啊:在DEVICE INFORMATION图中,X-FRM隔离变压器1,2,3,4端输入,5,6,7,8端输出,采用二极管冗余输出,输出接入LDO的IN端,然后被稳压至固定电压,该电压作为和原先VCC1完全隔离的电压VCC2可供其他元件工作(Supply to other Components)。
D1和D2是输出,我的意思是DEVICE INFORMATION中给LDO的输入。
哦,看来我的理解大致是对的哦,下面我想问的是D1\D2输出的电压是多大呢?是PWM波还是就是一个固定的电压呢?
不是PWM波也不是固定的直流电压, ISO1176T主要用于485总线的收发器,D1和D2是driver端的差分输出,