This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB940-Q1: patten 模式设置如何验证以及输出clock会变动问题

Part Number: DS90UB940-Q1


您好,现阶段有个项目线路流程如下:

现阶段检测由9211pattern输出模式屏能亮,而从845端输出的dsi信号正常,设置940的pattern模式,屏不亮,检测到9211有mipi输入,但输入到9211检测到从940输出的clk异常,是在变化的。
屏的具体参参数如下:

配置的940pattern如下:

//*ds90ub940 寄存器Pattern模式:

i2ctransfer -yf 3 w2@0x2c 0x66 0x00
i2ctransfer -yf 3 w2@0x2c 0x67 0x78
i2ctransfer -yf 3 w2@0x2c 0x66 0x01
i2ctransfer -yf 3 w2@0x2c 0x67 0x12
i2ctransfer -yf 3 w2@0x2c 0x66 0x02
i2ctransfer -yf 3 w2@0x2c 0x67 0x22
i2ctransfer -yf 3 w2@0x2c 0x66 0x03
i2ctransfer -yf 3 w2@0x2c 0x67 0x06
i2ctransfer -yf 3 w2@0x2c 0x66 0x04
i2ctransfer -yf 3 w2@0x2c 0x67 0x12
i2ctransfer -yf 3 w2@0x2c 0x66 0x05
i2ctransfer -yf 3 w2@0x2c 0x67 0x02
i2ctransfer -yf 3 w2@0x2c 0x66 0x06
i2ctransfer -yf 3 w2@0x2c 0x67 0x3B
i2ctransfer -yf 3 w2@0x2c 0x66 0x07
i2ctransfer -yf 3 w2@0x2c 0x67 0xE0
i2ctransfer -yf 3 w2@0x2c 0x66 0x08
i2ctransfer -yf 3 w2@0x2c 0x67 0x61
i2ctransfer -yf 3 w2@0x2c 0x66 0x09
i2ctransfer -yf 3 w2@0x2c 0x67 0x35
i2ctransfer -yf 3 w2@0x2c 0x66 0x0A
i2ctransfer -yf 3 w2@0x2c 0x67 0x06
i2ctransfer -yf 3 w2@0x2c 0x66 0x0B
i2ctransfer -yf 3 w2@0x2c 0x67 0x04
i2ctransfer -yf 3 w2@0x2c 0x66 0x0C
i2ctransfer -yf 3 w2@0x2c 0x67 0x14
i2ctransfer -yf 3 w2@0x2c 0x66 0x0D
i2ctransfer -yf 3 w2@0x2c 0x67 0x28

i2ctransfer -yf 3 w2@0x2c 0x6a 0x22
i2ctransfer -yf 3 w2@0x2c 0x6b 0x50
i2ctransfer -yf 3 w2@0x2c 0x65 0x04
i2ctransfer -yf 3 w2@0x2c 0x64 0xE1

  (1)请问一下我该如何验证pattern模式是否正确?

(2)940的输出clk异常是因为什么原因,还有我们能否通过寄存器的配置来设置940的mipiclock?如果有,具体设置哪些?

(3)能否帮忙提供一下940的初始化配置代码?

十分感谢!!!!