This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB935-Q1: BC问题咨询

Part Number: DS90UB935-Q1

你好!我最近正在调试一个新项目,加串为TI935,解串为TI954,根据935的规格书,其可以工作在多种模式,我将其配置为Non-synchronous Internal Clock,954可以正常出图,但是无法通过954通过FPDlink配置935(IIC),将935的模式配置为Synchronous模式,则954端无法lock。更换另外一个935的板子(别人家的),同步和非同步模式下可以正常工作。个人理解是我们板子FC通道是正常,但是BC通道异常,因为同步模式,935的clk是从BC过来的,非同步模式是935内部自己产生clk。这个问题可能的原因是什么?我们的TI935是单独供电,没有采用POC,Dout+端 AC电容为100nF,Dout- 端AC电容为47nF,COAX。

谢谢!