Part Number: DS90UB949-Q1
948设计是用Bist Pin启动BIST,我先在想使用949端的测试画面控制948显示,请问怎么可以控制停止948端停止自检画面;另外我切换949使用HDMI显示,948端可以正常显示
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB949-Q1
948设计是用Bist Pin启动BIST,我先在想使用949端的测试画面控制948显示,请问怎么可以控制停止948端停止自检画面;另外我切换949使用HDMI显示,948端可以正常显示
您好,可以直接将BISTEN拉低stop BIST。参考948的datasheet,用户可以自己控制BIST时间的长短,我想可以 使用主控的GPIO去控制BISTEN引脚的高低电平。

因为948端是客户设计的汽车仪表,我这边没法更改他们的设计,我通过远程I2C获取948端的0x24寄存器值为0x08,可以判断出他们是通过BISTEN pin控制的BIST,我是不是可以远程修改948端0x24寄存器只为0x00,这样是不是就可以关闭BIST
您好,远程修改寄存器0x24去enable或者disable都是可行的。
但是通常来说,要么通过硬件BISTEN去控制,要么都是寄存器去控制,BISTEN 引脚使能,寄存器去disable我认为也没问题。