Part Number: DS90UB933-Q1
Other Parts Discussed in Thread: DS90UB926Q-Q1
您好:
请问DS90UB933&DS90UB926是否可知支持帧率为50Hz,分辨率为1280×1024的图像传输;是否可以根据手册中的速率进行计算最大分辨率支持,若可以是否有计算公式可以直接进行计算呢?感谢解答。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB933-Q1
Other Parts Discussed in Thread: DS90UB926Q-Q1
您好:
请问DS90UB933&DS90UB926是否可知支持帧率为50Hz,分辨率为1280×1024的图像传输;是否可以根据手册中的速率进行计算最大分辨率支持,若可以是否有计算公式可以直接进行计算呢?感谢解答。
您好,
DS90UB933-Q1是DVP 接口产品,Image sensor 输出的数据除了active 的图像区域,也包含blanking 的数据。因此要准确计算PCLK,除了要需要知道resolution,也还需要知道具体的Blanking 的参数,然后利用下面链接中公式(1)或公式(2)进行计算。如果在初期选型阶段,不确定image sensor 的最终参数,利用公式(3)进行PCLK 预估,blanking time 取10%~15%即可。计算出来的PCLK 在FPDLINK 产品定义的PCLK 范围内即可。
https://www.ti.com.cn/cn/lit/pdf/zhcaa76
请注意,DS90UB926Q-Q1属于IVI(车载娱乐系统)产品 ,而 DS90UB933-Q1属于ADAS(自动驾驶)产品,它们不能搭配使用。
926和925可以搭配使用;933和934也可以搭配使用。
您是要用在什么应用场景,是Processor传输图像到显示屏,还是图像传感器或摄像头采集图像进行传输到Processor?还是前者是IVI的应用,后者是ADAS的应用。
926和925是IVI产品,933和934是ADAS产品。
如果是IVI应用,926是RGB接口,是一个时钟信号对应一个像素点。如果显示屏的blanking time不确定的话,可以按照10~30%的裕量进行估算:1280×1024x50x[1+(10~30%)]≈72.1MHZ~85.2MHZ
926的 PCLK 最大到85MHZ,因此如果所选显示屏的实际像素为72.1MHZ<85MHZ,那么926是满足要求的;所选显示屏的实际像素为85.2MHZ,那么它是大于85MHZ的,926是不满足要求的。925和926的PCLK 范围是一样的,都是5~85MHz。