请问5V的CAN与3.3V的CAN(TCAN334)通过CANH与CANL接在一起,3.3V的TCAN334是否会出现latch up的问题?能否附上TCAN334可靠性测试中,latch up的测试电压?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问5V的CAN与3.3V的CAN(TCAN334)通过CANH与CANL接在一起,3.3V的TCAN334是否会出现latch up的问题?能否附上TCAN334可靠性测试中,latch up的测试电压?
您好,在同一个CAN总线上可以将5V供电和3.3V供电的CAN收发器互连,这是因为它们的输出电压幅值差不多(比如60ohm阻抗显性状态下,都是>1.5V 差分电压)。并且输入阈值显性:>900mV,隐性<500mV).
这里有一篇关于CAN总线上如何将不同供电电压类这两种不同类型的收发器互连的,以及通过使用split termination的方法来降低不同供电电压对共模噪声的影响:https://www.ti.com/lit/an/slla337/slla337.pdf