Other Parts Discussed in Thread: TUSB215
问题点1:使用了TUSB215Q芯片的产品在通讯中出现通讯异常(Carplay和Carlife功能失效),请问导致失效的原因有那些?
问题点2:TUSB215Q芯片在通讯中数据无法建立连接(Carplay和Carlife功能失效),如果数据有连接上汽车日志可以记录到,现在汽车没有记录到通讯连接,是不是TUSB215Q受到什么干扰而导致通讯失败?
1.使用的场景是汽车主机+LVDS线束(100Ω,线束长度850mm~2000mm)+有TUSB215的产品+手机,通讯实现Carplay和Carlife功能,
2.TUSB215Q芯片的设计原理图
D2M/D2P连接到输入端接口,同时D2M/D2P也连接到输出端(type c口),就是说产品输入端和输出端的D2M/D2P是相通的(TUSB215Q的5/6号引脚搭在了D2M/D2P信号线上),VBI是VBUS(5V),TUSB215Q to EQ= Level 3/DC boost=40 mV Low,
3.我们也使用TUSB217Q芯片设计的产品,TUSB217Q芯片的产品就没有出现通讯异常的情况,TUSB217Q to EQ= Level 2
下图是TUSB217Q芯片的设计原理图,