Other Parts Discussed in Thread: SN65MLVD040,
两个SN65MLVD040可不可以当成SN65MLVD080使用?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
两个SN65MLVD040可不可以当成SN65MLVD080使用?
您好,可以的。因为每个通道的driver和receiver都有独立的使能端DE和/RE端。
040和080的区别主要在于040 集成了失效保护,多了一个FSEN 使能端以及PWDN引脚。
手册里这样描述,我想问一下这个Tpye1和Type2是什么意思?如果芯片正常工作,我理解是需要将FSEN拉低,PWDN拉高,是这样吗?
Failsafe enable pin. When this pin is left floating, internally this pin will be
pulled to logic HIGH.
This pin enables the Type 2 receiver for the respective channel.
xFSEN = L→Type 1 receiver inputs
xFSEN = H→Type 2 receiver inputs
您好,type1 和2的主要差异在于type2的差分信号不是以0V为共模电压的,有个直流偏置。如下图:
FSEN选择低还是高,主要取决于Vid的电压范围,您可以直接参考datasheet Table1的真值表。比如如果Vid>35mV, 那么FSEN=L,如果Vid>135mV
,则FSEN=H。 PDN引脚低有效,所以您的理解是对的,器件正常操作时,PDN需要拉高,normal operation 状态,否则PDN=L,输出高阻抗。
如果需要receiver 一直使能的话,可以直接接GND。
或者可以将DE和RE/ 接在一起,通过控制器来控制它的高低电平。
当为高的时候,DE enable,driver工作,receiver disable。当为低的时候,RE enable, Driver 端disable,receiver 工作。
driver端的输出A和B都接在了recevier端的输入上,所以是半双工的。driver和receiver 同一时刻只能一个工作。所以可以将DE和RE接在一起。某一时刻只能DE或者RE有效。