This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB964-Q1EVMTDA: 关于同步信号配置,及TESTEN PIN脚问题及多组Camera驱动问题

Part Number: DS90UB964-Q1EVMTDA
Other Parts Discussed in Thread: DS90UB964-Q1

1:可以通过配置GPIO[7,0]口来达到一对一驱动Camera?如果可以GPIO输入什么样的电平信号?

2:同步信号部分,第一种由外部向hub发送FrameSync,第二种为DS90UB964-Q1内部寄存器产生,那么内部寄存器产生的FrameSync可以通过什么方式配置才能达到与系统同步?

3:REFCLK部分,TESREN pin  SPEC中要求This pin should be tied Low, 为什么参考电路中接在无源晶振一端?

  • 您好,首先测试引脚TSETEN是一个测试点,参考电路中是独立下拉到地的哈,并没有和无源晶振一端接一起。

    关于您的第一问,我不太明白您的问题,964是可以同时接四路camera的,您这里指的一对一驱动,具体是什么意思?

    第二个问题,关于帧同步,如果使用内部帧同步,它对于964连接的4个camera来说是非常确定的,如果使用它通过GPIO输出到系统中的其他器件, 会增加一些不确定性,比如jitter。

  • 1:  第一个问题我的意思是比如4camera,现在只想驱动其中某一个camera工作,能否通过给与一个电平触发信号到964中某一个GPIO。从而实现一个GPIO控制一路Camera,

      2:用CPU一路I2C可以挂两个FPD-LINK HUB么?两个IC I2C地址可以设不一样吗?

  • 您好,

    1)我还是不太明白,即使使用964的GPIO透传到serializer的GPIO,然后接到Camera的什么引脚去控制它呢?如果您只使用一个camera的话,可以将其他通道disable。

    2)通过IDx的上下拉电阻值的不同可以使得一个I2C总线上挂接8个hub,这8个地址肯定是不同的,如果是相同的,就会发生总线仲裁。

    详见数据手册的8.5.1 Serial Control Bus部分的介绍。