Hi,TI
948的CMLOUTP和CMLOUTN是眼图测试引脚,COAX模式的眼图可以用这两个引脚来测试吗?
还请帮忙确认,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,测试眼图我们建议是差分配置,使用STP,示波器使用差分碳棒,并且外部端接100ohm终端匹配电阻,如果示波器已经端接匹配电阻,则外部不需要。
如果要使用单端coax cable,要按照下面连接方式将RIN-通过50ohm电阻接GND。
您好
SER的Dout和DES的RIN是按照COAX模式接续的。
948的眼图测试点仍然是CMLOUTP和CMLOUTN吗?
如果是的话,还需要串电阻吗,阻值多大?
如果不是,还请告知测试点和测试方式。
CMLOUTN 类似于RX的接法,接50ohm到GND,只使用CMLOUTP端进行测试。