This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB953-Q1: DS90UB953TRHBTQ1使用

Part Number: DS90UB953-Q1


当前在做输电线路监拍仪升级项目,主要是摄像头升级由原来的800W升级到1600W,客户想选一款连接摄像头和MCU的串行器,客户之前200W和800W有评估过DS90UB953TRHBTQ1和DS90UB954TRHBTQ1,麻烦问一下两颗芯片能否支持1600W 30fps?另是否有其它芯片推荐,谢谢

  • 您好,1600w分辨率是不是4928×3264? 如果是的话我们可以计算下数据的吞吐量:以RGB888 24bit 色深,25%消隐时间为例:

    4928*3264*30*24*(1+25%)=14.48Gbps。如果YUV422 10bit的数据格式,就把这里的24改成10去计算下。

    而DS90UB953最大可支持的data throughout为3.328Gbps。只要计算下来小于3.328Gbps就是可以支持的,因此如果是24bit, 1600w,30fps的分辨率是不支持的。