This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!如标题配置,我们这边调试CH0-CH3单独输出图像都没问题,请教下如何设置可以同时输出CH0-CH3
查阅手册有些部分有介绍,但是不太懂,参考了以下示例Code设置目前也不能输出4路图像,请帮忙指点下!谢谢!
Code Example for Line-Interleaved CSI-2 Forwarding
# "*** RX0 VC=0 ***"
WriteI2C(0x4c,0x01) # RX0
WriteI2C(0x70,0x1f) # RAW10_datatype_yuv422b10_VC0
# "*** RX1 VC=0 ***"
WriteI2C(0x4c,0x12) # RX1
WriteI2C(0x70,0x1f) # RAW10_datatype_yuv422b10_VC0
# "*** RX2 VC=0 ***"
WriteI2C(0x4c,0x24) # RX2
WriteI2C(0x70,0x1f) # RAW10_datatype_yuv422b10_VC0
# "*** RX3 VC=0 ***"
WriteI2C(0x4c,0x38) # RX3
WriteI2C(0x70,0x1f) # RAW10_datatype_yuv422b10_VC0
# "CSI_PORT_SEL"
WriteI2C(0x32,0x01) # CSI-2 select
# "CSI_EN"
WriteI2C(0x33,0x1) # CSI_EN & CSI-2 4L
# "*** CSI_SYNC_FWD synchronous forwarding with line interleaving ***"
WriteI2C(0x21,0x28) # synchronous forwarding with line interleaving
# "*** FWD_PORT all RX to CSI"
WriteI2C(0x20,0x00) # forwarding of all RX to CSI-2
您好,962接了四个UB933,然后前端接了4个camera是吗?
962的0x0C寄存器怎么配置的,是否将每个RX port都enable了?如果都enable了,那么建议您做下面尝试:
1. 同时接两个camera看是否能同时输出?
2. 同时接三个camera看是否能同时输出?
3.如果接两个可以,接三个不可以,或者接两个,三个都可以,同时接四个不可以,那是和962的带宽有关。
camera是多大的分辨率?
hi Kailyn,非常感谢您的支持!
0x0c寄存器配置为0x0f,同时接两个以上就不能出图了,单个camera最大分辨率就是1280*720*30fps,YUV422 8bit输出。
另外讲下我的视频接收器是需要先配置图像的分辨率的,也有可能是我分辨率配置不对导致放不出图像,如果接4个camera,那么我怎么确定图像如何排列的
看手册中这两个图片介绍我如何确认我的camera是如何排列的呢?
谢谢!
您好,这两种排列方式可以通过寄存器0x21去配置:
另外,我按照8bit YUV422 1280*720*30fps计算,并没有超过962的最大带宽,所以四路应该是同时可以支持的。
不必客气,那我暂时先把这个帖子关闭了,后续有什么问题,再跟进。
hi Kailyn:
我们的摄像头已经可以4路同时输出了,但是图像输出20S左右就会断开,这种现象有没有什么地方可以排查呢?
请问您和https://e2echina.ti.com/support/interface/f/interface-forum/224437/ds90ub962-q1-ds90ub962-q1-953-4-2中的问题是不是同一个问题?
如果是的话,我会在上述链接中跟进这一个问题。