Other Parts Discussed in Thread: LMK00308, LMK03806
看芯片LMK00308芯片手册,想用LVDS输出50MHZ的波形,但是看到手册中,LVDS接口只标明了最大输出频率为1.0-1.6GHZ,请问从哪里可以知晓最小输出频率,且LMK00308作为时钟缓存器,是不是出入多少频率,就会输出多少频率。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不知你的具体应用是什么,输入多少?LMK00308当Vod>=250mV时,输出频率最小为1GHz。
需要参考输入,但输出频率的范围要看你配置成哪种输出,比如是LVPECL,LVDS,还是HSCL,LVCMOS输出,不同的输出,输出最小频率值也不同。
左边的频率值指的是信号频率,可以理解为载波频率,右边的频率值指的是距离载波频率的距离,相位噪声值您理解的是正确的,-156比-130的表现要好,并不是比较所谓的绝对值。