近期从ti申请的样片iso1050在做CAN通信时出了问题 ,iso前级(从MCU到iso有CAN信号)但是在后级就检测不到信号了。请问什么情况可能导致这样的问题?谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
近期从ti申请的样片iso1050在做CAN通信时出了问题 ,iso前级(从MCU到iso有CAN信号)但是在后级就检测不到信号了。请问什么情况可能导致这样的问题?谢谢!!!
Yongwei li,
您好,您电路里面的TVS管我没看错的话应该是没有接到CANH和CANL吧?请您再确认下
从你的描述看,目前是MCU有发送出信号,但经过ISO1050后,总线上没有信号,对吗?
你总线上有其他CAN设备吗?如果他们往总线上发送信号,ISO1050的接收正常吗?
如果都没有,
1. 检查VCC1 和VCC2是否正常?检查信号时,要直接量到pin脚上看。
2. 如果总线上没有其他设备,尝试MCU发送信号,请把MCU发出的波形发出来看看(量ISO1050的TXD引脚)