Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: LMK05318B
目前使用单dsi输入,0x56寄存器配置为0x01,目前显示有轻微抖动,是因为外部时钟和dsi频率对不上的缘故么。
屏幕参数为2240*1260,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Other Parts Discussed in Thread: LMK05318B
目前使用单dsi输入,0x56寄存器配置为0x01,目前显示有轻微抖动,是因为外部时钟和dsi频率对不上的缘故么。
屏幕参数为2240*1260,
使用外部参考时钟模式,注意一定要使用低抖动时钟源。
使用mk05318b 产生时钟作为参考时钟的话,如果您是使用lmk05318b 的PLL2作为clock generation输出的话,PLL2的底噪比较高,所以输出jitter比较大。
对于lmk05318b这颗时钟器件来说,PLL1内部集成DPLL,而DPLL又是由数字环路滤波器组成的,所以PLL1 适合作为jitter cleaner。
所以显示轻微振动,很有可能是参考时钟源的jitter 导致。
DS90UB941手册中提到使用external clock reference,有 clock jitter 要求,
| fPCLK / 40 < Jitter frequency < fPCLK / 20, TJ@BER<1E-10 |
lmk05318b 的pll2能否输出满足这个要求的频率呢,抖动在180.25Mhz下大概为88ps

按照下面note(1)的公式我们可以计算下,
dual link mode: (1/(35*180.25MHz/2))*0.28 =88.7ps。
您目前使用的lmk05318b 作为外部参考时钟源,是否有测试它的jitter是否有超过88ps?
需要带有jitter分析功能比如DPOJET软件的高速示波器可以测试。
这里有一篇关于如何测量jitter的应用手册,希望对您有所帮助: