This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65987D: TPS65987D works with HD3SS460, no DisplayPort signal output

Part Number: TPS65987D
Other Parts Discussed in Thread: HD3SS460

Hi TI team,

We have a project that used TPS65987 and HD3SS460 to implement DP ALT mode on the Source side. The schematic is attached.

typec_ti.pdf

Now the TPS65987 can be programmed by the Application tool. And the PD status works fine (5V/3A is good), and the UFP device can be detected when making a TypeC monitor plugged.  But no Displayport signal output!!!The program project file is attached.

test_tps65987.pjt

Using the Application tool debug mode, below are some screenshot for reference.

Looking forward to your response. Thanks!