This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDA-050047: TPS25750+BQ25792

Part Number: TIDA-050047
Other Parts Discussed in Thread: TPS25750, BQ25792

我参考TIDA-050047进行设计,调试过程发现如下问题:

1.用TPS25750 Application Customization Tool工具进行配置,然后Flash到EEPROM内,上电后IIC总线上最后一组数据为向0x6b地址的0x0a寄存器写入0x00 0x00(该地址为bq25792的寄存器)导致错误配置bq25792的输出电压及其它参数(SYS应该为8.4V实际输出3.5V即将2S电池配置为1S电池),实际并未配置0x6b地址的0x0a寄存器的内容。请问 Application Customization Tool生成的配置文件有错误还是配置方法有问题?该如何用 Application Customization Tool配置?

2.BQ25792在电池欠压保护后(输出0V),充电电压为2.3V(无法达到激活过放电池需要的6V以上电压,bq25792采用硬件默认配置为2S电池)请问如何提高电池欠压保护后的充电电压以激活电池充电?

  • HI

       首先要确认数据是否保存到eeprom中,然后示波器再确认i2c上数据是否传给BQ25792?

       关于电池的问题,建议你放到电池论坛,会有对应工程师帮到你。

x 出现错误。请重试或与管理员联系。