This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB948-Q1: DS90UB948 電路設計要點

Part Number: DS90UB948-Q1


Dear teams,

長久以來感謝您的協助,我這裡有一些948設計上遇到的問題,再麻煩您協助解惑,謝謝!

1. DS90UB948是否有高速的GPIO用作backligth PWM(10KHz max),是否標註有High speed的即可?目前使用pin11是否可以?

2. DS90UB948與Audio PA I2S連接使用的是slave,請問是否OK?

3. DS90UB948 I2C是否只能作為host,地址配置應注意什麼,如圖是否OK? 是否可以做主機控制觸摸屏及Audio PA

Best Regads,

Rookie

  • 1.您好,GPIO分前向通道forward channel和后向通道back channel。 前向通道GPIO的带宽取决于PCLK的采样频率, 一般不超过PCLK的1/4,比如40Mhz的PCLK频率,那么GPIO最大频率为12Mbps。 而后向通道最大能支持的data rate 可直接参考下面表格。

    2.使用master还是slave mode,取决于搭配使用的serializer型号,其中SS mode即为Slave mode,Auxiliary mode为master mode:

    3. I2C的地址取决于IDx的上下拉电阻阻值,您这里使用上拉40.2Kohm,下拉49.9Kohm,对应的7bit从机地址为0x38. 使用这8 个地址中的任意一个都可以的。