Other Parts Discussed in Thread: LMH0395
你好!
现在想做HD-SDI远距离传输,目前有一款现成的解串器和串行器电路板,不过是MAXIM的GMSL系列的MAX9259和MAX9260。想匹配贵司的中继器进行远距离传输(>200m),是否能够推荐一个好的中继方案。附件是MAX9259和MAX9260的datasheet。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMH0395
你好!
现在想做HD-SDI远距离传输,目前有一款现成的解串器和串行器电路板,不过是MAXIM的GMSL系列的MAX9259和MAX9260。想匹配贵司的中继器进行远距离传输(>200m),是否能够推荐一个好的中继方案。附件是MAX9259和MAX9260的datasheet。
你可以考虑LMH0395这款HD-SDI的cable driver: Equalized Cable Lengths (Belden 1694A):200m at 2.97 Gbps, 220m at 1.485 Gbps, and 400m at 270 Mbps。
应该能满足你的需求,参考下它的数据手册:http://www.ti.com/lit/ds/symlink/lmh0395.pdf