Part Number: DS90UB941AS-Q1
Dear teams,
感謝您的幫忙!想請教您幾點問題:
- 是否我可以只用DSI0 or DSI1, 如果支援WUXGA這樣我DOUT 需要2 lan嗎?
- 是否我接DSI0 和 DSI1, 如果支援WUXGA, 這樣我DOUT 可以接 2個panel ?

Best Regards,
Rookie
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90UB941AS-Q1
Dear teams,
感謝您的幫忙!想請教您幾點問題:

Best Regards,
Rookie
是否我可以只用DSI0 or DSI1, 如果支援WUXGA這樣我DOUT 需要2 lan嗎?
可以只使用DSI0 或者DSI1,您这里指的DOUT 需要2lane,指的是941的FPD link这里是DOUT0和DOUT1是否都要输出是吗?
- 是否我接DSI0 和 DSI1, 如果支援WUXGA, 這樣我DOUT 可以接 2個panel ?
DSI0 和DSI1都接,那就是dual DSI input, 前端音频源是两个还是一个输入?如果是一个视频源输入,那么使用DSI0和DSI1,那么每个像素时钟需要一半的频率。
根据您的描述,您应该是下图中的应用吧?

Dear Kailyn,
謝謝您的協助! 沒錯,最終我要選擇這個模式。想請問一下2個頻幕都是1080p with 30fps (1080p/30fps/24bit)也ok嗎?

Best Regards,
Rookie
Hi Rookie,
那您这边是想把什么分辨率的视频spit两个1080p 30fps的显示?即红色部分是个什么分辨率的图像?941的每个link支持105Mhz,而1080p30fps需要的PCLK为75Mhz,所以如果想分离两个1080p30fps的图像,则PCLK需要150Mhz,是支持的。