This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD12S016: 有IIC输入信号没有输出信号

Part Number: TPD12S016
Other Parts Discussed in Thread: AM5728,

   HI

  主控采用AM5728,IIC经过TPDA2S016,再到HDMI接口,如图所示,目前出现出现的问题是:AM5728有IIC波形输出到TPDA2S016,波形如图所示,TPDA2S016没有波形显示,TPDA2S016电压正常,请问是芯片连接了防护需要做模式处理吗?

 

  • 目前做的工作:芯片TPD12S016已经替换了新的,还是没有反应;又将TPD12S016相连接的D0到D2正负六根线去掉,还是没有波形,最终导致屏幕界面下移,屏幕上方会有一块黑块,请问怎么解决,

  • 您好,

     HDMI controller芯片的供电电压是多少?VCCA要与它的供电电压一样;

    LS_OE和CT_HPD内部应该有下拉,实测下这两个管脚的实际电压是多少?是否为高电平?

    5 V_OUT是否有输出,电压是否正常?

  • HI

    测试LS_OE为低和CT_HPD为高,VCCA供电3.3V,MCU供电3.3V,5V电压输出正常5.04V

  • LS_OE需要是高电平才能使能电平转换,您将LS_OE设置成高电平看是否可以解除问题

x 出现错误。请重试或与管理员联系。