Other Parts Discussed in Thread: DS90UB941AS-Q1,
Serializer:DS90UB941AS-Q1,使用DSI0
Deserializer:DS90UB948-Q1,使用dual link
目前941的DSI没有接输入,屏幕有背光但无显示,想通过948的Pattern Generation输出1080p60hz的测试画面,应如何配置948的寄存器?要使用948自己的内部时钟源。
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Serializer:DS90UB941AS-Q1,使用DSI0
Deserializer:DS90UB948-Q1,使用dual link
目前941的DSI没有接输入,屏幕有背光但无显示,想通过948的Pattern Generation输出1080p60hz的测试画面,应如何配置948的寄存器?要使用948自己的内部时钟源。
Thanks!
您好,如果使用deserilazer端即948的内部时钟源,那么双向控制功能是无效的,如果想通过941 的I2C去控制948的话,需要使用外部时钟。
另外,pattern test的配置有以下几种,
第一,没有外部时钟,使用的是941内部的时钟源,并且PAGTEN是serializer 端enable的。
第二,外部时钟源,deserializer端的PATGEN 由local I2C 使能的。
第三,只使用deserilaizer,local I2C,使用内部时钟源。

我们已经能够产生colorbar了,但是有另外的问题请教:
1、现在使用内部时钟产生colorbar时,M=7,N=0x28,pclk=(800*7/40)=140M,而1080p的pclk=2200*1100*60=145.2M,所以我们的M/N设置是否是合理的?
2、到实际应用时,我们BRIDGE_CLK_MODE=01: External Reference Clock Mode,硬件设计上External Reference Clock是一个25M晶振,此时的M/N应如何设置呢?
Thanks!
现在使用内部时钟产生colorbar时,M=7,N=0x28,pclk=(800*7/40)=140M,而1080p的pclk=2200*1100*60=145.2M,所以我们的M/N设置是否是合理的?
1080p60fps的分辨率需要PCLK要148.5Mhz。所以如果M=7, 配置N的寄存器0x23=0x28的话,计算下来PCLK=140MHz是不能支持1080p的分辨率的。
建议将M/N 的divider稍微大一些配置。
到实际应用时,我们BRIDGE_CLK_MODE=01: External Reference Clock Mode,硬件设计上External Reference Clock是一个25M晶振,此时的M/N应如何设置呢?
M/N 的divider是针对使用内部晶振时使用的,如果配置为外部参考时钟,那么M/N则不需要配置。 可以使用默认值。