Hi Kailyn Chen ,
你好!
941产生pattern时,使用内部200M的,可以正常工作。但是配置成800M时,没有视频信号输出。800M时的寄存器配置如下:
{0x66,0x03},
{0x67,24},//N
{0x66,0x19},
{0x67,2},//M
要怎么配置,才能使用内部800M?
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kailyn Chen ,
你好!
941产生pattern时,使用内部200M的,可以正常工作。但是配置成800M时,没有视频信号输出。800M时的寄存器配置如下:
{0x66,0x03},
{0x67,24},//N
{0x66,0x19},
{0x67,2},//M
要怎么配置,才能使用内部800M?
谢谢!
您好,是DS90UB941吗? 那应该配置的是寄存器0x1A的M值,如果M 配置为1,则默认使用的是200Mhz当M的值大于1的时候,相当于enable 内部800Mhz。