This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB941AS-Q1: Dual-DSI Input Mode

Part Number: DS90UB941AS-Q1


Hi,TI

现在想使用联屏方案是,用一块27寸屏幕推两幅画面(主驾和副驾屏),分辨率为4032*756,两幅画面各占一半2016*756

LCD屏幕的接口是dual-LVDS,帧率为55Hz,扫描方式是奇偶扫描。总的PCLK=177.26MHz

在941式样书中看到这两个模式,两个模式都可以实现我们想要的应用场景吗?

没有理解这两个模式

1. 其中图8-13,图8-14的解串器接的LCD屏幕,扫描方式都是奇偶吗?

2. 图8-13的解串器是如何识别941进入的奇偶信号?

3. 这两图的解串器都可以是948吗?

4. 两种模式,都是在DSI0和DSI1输入到941后,941将它们合成一个画面,然后通过解串器(例:948)解成dual-LVDS,dual-LVDS是奇偶模式?