This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,问题1:cdce62002输出的时钟与参考时钟能否同频同相呢?
问题2:目前我只需要两路单端的时钟输出,那我应该怎么接?使用一个差分out的P/N呢,还是接成两个out的 P端?
1.可以同频,但是不保证同相.
2.可以LVCMOS,一个p,一个n
CDCE62002 的输入时钟: REFP(单端的参考时钟)和 AUX_IN(晶振时钟输入) 在EVM板上串接了一个0.1uF的电容,这个电容的作用?必须要这样做吗?