AM26LS31的输入能直接连stm32的io口吗,是否需要串个电阻或者三极管之类的?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
AM26LS31是差分输出,您是使用单端输出吗?AM26LS31也可以单端输出,差分输出的另一个管脚可以浮空;
但是AM26LS31供电范围典型值是5V,您使用的stm32是几伏供电,I/O口电平范围是多少?

请注意 AM26LS31的管脚定义,16脚封装的IC,其pin4是G;pin13是4Z;pin15是4A,如下截图定义:

其封装可以在其产品主页,按如下指示下载:
AM26LS31产品主页链接:https://www.ti.com.cn/product/cn/AM26LS31

抱歉,我看错了您的问题,我误以为您要使用stm32的io口接收AM26LS31的输出信号;
AM26LS31可以接收3.3V的电平,它的输入管脚不会有接近5V的电压,它是输入管脚,除非有其他ESD
对于AM26LS31,不使用的输入A管脚建议通过4.7K电阻接VCC;因为这些电阻在嘈杂环境中工作可以时提供输入电流限制。 通常,意外的噪声瞬变会上升到高电压水平,对未受保护的输入可能致命。不使用的输出可以悬空;
对于AM26LS32,将未使用的同向输入A通过4.7K上拉电阻器连接到Vcc,将未使用的反相输入B通过4.7K下拉电阻器连接到接地。不使用的输出可以悬空;
具体见下面附件解释: