您好,在使用到芯片LMK04806时,输出100M,2.5M,40M,50M的频率,且这些频率必须同步,不允许有相位差,是不是只需要用SYNC就可以实现呢,看到datasheet中介绍到digital delay,它的设置涉及到SYNC的配置,还是不同的频率输出相位会有差,需要设置不同的digital delay 呢?麻烦解答一下,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,在使用到芯片LMK04806时,输出100M,2.5M,40M,50M的频率,且这些频率必须同步,不允许有相位差,是不是只需要用SYNC就可以实现呢,看到datasheet中介绍到digital delay,它的设置涉及到SYNC的配置,还是不同的频率输出相位会有差,需要设置不同的digital delay 呢?麻烦解答一下,谢谢!
1. 输出同步直接参考手册41页图7-2,Figure 7-2. Clock Output synchronization using the SYNC pin (Active Low)。此情况下各通道digital delay设置成同样的值,或者都用默认值即可满足你的应用。
2. Digital delay的参考源是时钟分配路径上的那个最高频时钟,而不是输出时钟。参考手册42页图73,Figure 7-3. Clock Output synchronization using the SYNC pin (Active Low)。你的应用里,如果在PCB布板会引入一些通道间的skew,则可以考虑用digital delay或者analog delay补。如果确认PCB布板不会引入太大的skew,则可以不用太过考虑digital delay。