This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK04906 芯片资料上写支持1KHz的参考输入,但是LOS_TIMEOUT检测最低频率是420khz,如果参考输入低于420khz(1khz)会直接los无法锁定了吧?这请高手指教,多谢~



因为有LOS_TIMEOUT的存在,是不是说输入参考时钟只能大于420khz?谢谢指导

  • 你好!

    LOS_TIMEOUT是设置一个时间值的,即检测到多久没信号后就告警。

    “This bit controls the amount of time in which no activity on a CLKin causes LOS (Loss-of-Signal) to be asserted.”

  • 我的理解是:由于LOS_TIMEOUT是必选项,而且420khz是最大的检测周期,即1/420ms内如果检测不到脉冲后就报丢失,但是如果是1khz的输入,就意味着1ms才有一个脉冲, 那肯定会报丢失了,无法锁定。如果这样分析下来,LMK04906应该不能使用低于420khz的参考输入时钟对吗?还是说可以不使能LOS_TIMEOUT检测功能?

    不知道我理解的是否有误,请帮忙指导一下,多谢~

  • 1. 为什么LOS是必选项?EN_LOS disable掉,不就没有LOS这个功能了么?

    2. 为什么要用1KHz的输入?实际应用中从来没有见过有哪家客户的哪个项目,会用到KHz级的参考输入。用得比较多的,反倒是122.88M,125M之类的参考用得很多。

  • 正如上面的同事所讲,LOS_TIMEOUT这个功能是可以disable的。

    由于芯片内部只用到2bit的寄存器来设置LOS_TIMEOUT,最小值为420kHz,所以对于低于这个值得输入时,是需要进行disable掉这个功能的。

    对于kHz级别的参考输入,一般是在有线通信上有。你需要这么低的输入吗?

  • 明白了,非常感谢