Other Parts Discussed in Thread: LMK04806
您好:我想问下LMK04806的LEuwire,CLKuwire,DATAuwire以及status_LD,status_holdover评估板上是通过电阻接到一个header上(这些电阻的作用是什么),如果是想把这些接到一个host上,不知如何去接,可以参考评估板上的电路吗。谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: LMK04806
您好:我想问下LMK04806的LEuwire,CLKuwire,DATAuwire以及status_LD,status_holdover评估板上是通过电阻接到一个header上(这些电阻的作用是什么),如果是想把这些接到一个host上,不知如何去接,可以参考评估板上的电路吗。谢谢。
评估板上加分压电阻的目的是为了和电脑5V的LPT 端口连。
如果你是和3.3V逻辑的MCU相连的话,就不需要这些电阻。不过保险的话,建议在走线上串联一个小电阻。
具体接法: MCU---PCB走线---电阻(33Ω)---PCB走线---LMK
你好,请问你你也使用过LMK04系列时钟芯片,有问题可以单独我们工程师交流吗,可否把邮箱或者微信,联系电话发到我邮箱1353183164@qq.com中