This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求教!!锁相环74HC4046芯片电路连接问题!!!!

网友 lzb124548443 在21ic 模拟技术 论坛问以下问题:

http://bbs.21ic.com/icview-581818-1-1.html

如图,左面为VCO,右面为鉴相器
当断开VCO芯片9脚VCOi处导线时(图中红色导线),测得鉴相器输出相位差电压为3V,当一连接上此导线,相位差电压为零。为什么会发生此现象?
而用PC3鉴相器则没有此现象!求大神指教!

  • 你检查一下是不是两种鉴相器的输出逻辑不一样。按说在锁定的时候,相位差为0是没问题的啊。

    另外,C67,R73,C68,R67是环路滤波器么?看上去这个滤波器接法也不对,典型的滤波器接法是VCOi接C68到地,然后VCOi接C67串R73到地,你检查一下。还有R67=100K是不是太大了,如果用作整数PLL,这个电阻可以改成0欧姆;如果用作小数PLL,这个电阻几百欧姆或者几K就够了。