This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
首先复位PHY,往0x00寄存器写0x8000;然后读0x00,内容为0x3100。读0x10,内容为0x0000;然后读0x01的0x0004位为0。程序如下:
do
{
timeout++;
} while (!(ETH_ReadPHYRegister(PHYAddress, PHY_BSR) & PHY_Linked_Status) && (timeout < PHY_READ_TO));
直到超时,0x01寄存器的第4位一直为0,请问怎么回事?PHY与RJ45连接,连接方式与官网参考电路一致。还有,想问一下那个LED灯怎么接?具体电路如图所示。
我用的是Slave Master模式,Pin6应该是TXD3,应该是上拉吧。。。我把TXD2下拉1k电阻了。那个RX_CLK,和TX_CLK有50MHz输出。。。CLK_OUT输出25MHZ,RX_CLK在复位时是25Mhz的时钟,请问这样我改如何调试?
您图中E\G是指的地吗?LED_LINK信号信号上电不是要被采样吗?我现在LED_ACT和LED_SPEED是按照您的接法连接的,只有LED_SPEED常亮,其他的不亮。。。
为什么我的MII_MODE脚接上拉了,可他的管脚还是低电平啊……?是不是芯片有问题啊?
还有就是,第40引脚(SRS_DV)不接上拉可以吗?
求快回……!谢谢了……!
你好!能帮我解答下这个问题吗?谢谢了…………!
http://www.deyisupport.com/question_answer/analog/interface_and_clocks/f/59/t/50941.aspx
恩恩,能不能帮我看看这个问题啊…………?谢谢了……!
http://www.deyisupport.com/question_answer/analog/interface_and_clocks/f/59/t/50872.aspx