This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于BQ32000请教各位大侠。

BQ32000是带有trickle charger功能的RTC芯片。

不知trickle charger是固定抬升VBAT电压到多大进行充电?

充电电流是脉冲式的吗,电流有多大?

我想VBAT接一个3.6V的纽扣锂电池,该锂电池同时给其他一个2~3.6V的低功耗芯片(GPS的备用电池电源管教)供电,是否可行?

如果不行,能否推荐其他简易方案,不会只能用专门锂电池充电芯片(充电电压到4.2V)+   2~4.2V转3.3V的电源模块(这个是否有推荐芯片)   来给RTC和GPS供备用电源吧?

谢谢~~