现在我使用TPS65987D做与显示器PDO协商
在使用 IIC 写 TPS65987D 的 0x33寄存器设置PDO的时候,需要断开CC信号重连,显示器那边才会重新协商到我设置的值,有没有什么办法不断开CC信号重而让他们重新协商输出到我设置的VBUS
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
感谢您对TI产品的关注!为更加有效地解决您的问题,我将您的问题发布在了E2E英文论坛上,将由资深的英文论坛工程师为您提供帮助,收到回复后,若有疑问您可以跟进英文工程师的回复:
E2E英文论坛工程师已回复:
After the 0x33 Sink Capabilities register has been updated, the customer can use the 'GSrC' 4CC command to force the connected device to re-send its source capabilities and renegotiate a new PD contract with the updated Sink Capabilities.
The flow would be as follows:
1. Updated Sink Capabilities in 0x33
2. Send 'GSrC' 4CC Command
3. New PD contract will be negotiated