This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SN75LVPE5412和DS320PR412的区别是什么?是可以完全替代吗?
您好,
DS320PR412已经停产了,无法再找到其datasheet,相关资料已从官网删去;但是DS320PR4xxEVM User's Guide用户指南中提到,在本文中,DS320PR412的所有实例都可以与SN75LVPE5412互换,DS320PR421的所有实例都可以与SN75LVPE5421互换。如下截图:
DS320PR4xxEVM用户指南:https://www.ti.com.cn/cn/lit/ug/snlu301/snlu301.pdf
因此,我认为像EVM中类似应用可以直接替代
上述截图表格是在 6.4 DC Electrical Characteristics 即直流电气特性表格中的截图,所示参数指的是Rx DC Single-Ended Impedance 和 DC Differential Tx Impedance都是直流参数;而85Ω是指的高频信号中的传输线的特征阻抗,我想这不是一个概念,在datasheet 中 8.2.1.1 Design Requirements章节也提到PCIe需要使用85Ω的特征阻抗线:
很抱歉,上面回复应该有误,我查到:传输线的特征阻抗是由传输线的结构以及材料决定的,而与传输线的长度,以及信号的幅度、频率等均无关。
我又在PCIE5.0规范中查到如下描述,即 PCIE1.0 2.0 3.0中 采用的是单端50Ω,差分100Ω特征阻抗,而PCIE 4.0 5.0是采用的单端42.5Ω,差分85欧姆特征阻抗。
SN75LVPE5412支持 PCIe 1.0, 2.0, 3.0, 4.0, and 5.0,电气特性表格中说的50Ω和100Ω应该针对的是PCIe 1.0, 2.0, 3.0,而 8.2.1.1 Design Requirements章节中提到的PCIe需要使用85Ω的特征阻抗线,这里指的应该是 PCIe4.0或PCIe5.0。